How to Prevent Food Contamination | Regal Rexnord
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
  2. Regal Rexnord Insights
  3. How to Prevent Food Contamination
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
How to Prevent Food Contamination

Edit

Conveyor with chicken in packaging


 

Food contamination is a serious concern in the food processing industry. Poor hygiene or equipment failure can lead to contamination. Contaminated food threatens the health of consumers and the reputation of the manufacturer. Contamination can happen at many points during production. Food manufacturers must take clear steps to protect their products.

Preventing contamination depends on strong sanitation practices, trained employees, and the right equipment. With these elements, producers can maintain clean operations and deliver safe food. 

How Contamination Happens in Food Processing Facilities

Food processing facilities handle raw ingredients and turn them into finished food products. These operations rely on advanced technology and automated equipment to work efficiently. However, when equipment is not properly cleaned or maintained, contamination risks increase.

Where does this risk come from? Chemicals, viruses and bacteria and many other contaminants pose these risks. Many facilities use automated conveyor systems in industrial assembly lines. You’ll see these lines in production, processing, packaging, and storage of any kind of food. If measures are not taken to ensure safety, contamination is possible. This is why hygiene and sanitation standards are so crucial.

Common Types of Food Contamination

There are several types of contamination that cause risks in food processing units. These include:

Microbial Contamination

Microbial contamination occurs when bacteria, viruses, or other pathogens enter food. This happens through dirty surfaces, contaminated water, or improperly handled raw ingredients.

Chemical Contamination

Chemical contamination happens when harmful substances enter food products. These chemicals may include cleaning agents, pesticides, or heavy metals like lead or mercury. Improper storage or misuse of chemicals can quickly create food safety hazards.

Packaging Contamination

Packaging contamination occurs when food comes into contact with contaminated packaging materials. These can include printing inks, adhesives, or bacteria. An example would be food getting contaminated during packaging from:

  • The packaging equipment being dirty (such as oil or grease from the machines).
  • Exposure to foreign matter such as dirt, dust, insects, glass, etc.
  • Direct or indirect contact between the handler and the food. This could even include an instance such as the handler’s jewelry falling into the food.

Personnel Contamination

Personnel contamination happens when food handlers transfer pathogens to food. This could happen through skin, hair, clothing, or bare hands. Poor personal hygiene or lack of proper training increases this risk. Employee procedures are a central part of food safety programs.

Best Practices for Preventing Food Contamination

Preventing food contamination requires a coordinated approach. Both procedures and equipment are key to fighting contamination.

For guidance, consult the FDA's Employee Health and Personal Hygiene Handbook. The handbook encourages best practices and behaviors. These can prevent food handlers from spreading viruses and bacteria to the product.

U.S., federal, state, and local regulations set sanitation standards for food production. Many of these standards call for regular cleaning of machinery. Prioritizing hygiene and sanitation in your facility is key to preventing food contamination. Good sanitation practices include regular washing and disinfection of the machines and conveyors.

Proper Washdown Procedures For Food Safety

Washdown procedures help remove bacteria, residue, and allergens from food processing equipment. These procedures often involve hot water, high pressure sprays, and chemical cleaners. However, washdown environments place heavy demands on machinery. This is especially true when cleaning happens daily or many times per shift.

Washdown schedules should:

  • Match product risk,
  • Train sanitation teams on proper pressure and chemical use, and
  • Establish a schedule to inspect equipment for signs of corrosion or moisture damage.

By planning washdown procedures, facilities can keep sanitation consistent and protect equipment.

Washdown Ready Equipment for Food Processing

Not all processing equipment can withstand frequent washdowns. Motors and components in food plants must resist moisture, chemicals, and bacterial buildup. Knowing how to choose a washdown motor helps food processors select equipment. Factors include enclosure design, sealing methods, and corrosion resistant materials.

Washdown ready equipment often features stainless steel construction. Stainless steel is water and contaminant-resistant. Other factors to look for include smooth surfaces and sealed housings. Smooth surfaces can prevent buildup. Sealed housings can keep contaminants out of equipment. Choosing the right equipment supports food safety while reducing downtime and repair costs.

Use Reliable Washdown Duty Motors

Motors are often installed close to food contact areas. Because they're a key part of food production, their design is critical. LEESON® Motors is a leading manufacturer of washdown motors. The LEESON approach focuses on:

  • Sealing out moisture,
  • Eliminating areas where bacteria can grow, and
  • Using durable materials that perform during frequent cleaning cycles.

Washdown motors reduce the risk of corrosion, condensation, and seal failure. Washdown features help maintain sanitation standards while supporting consistent and dependable operation.

Understand IP Ratings and IP69K Protection

Protective standards help determine how well equipment keeps out water and contaminants. One of the most common is the Ingress Protection (IP) rating. IP ratings describe a product’s resistance to dust and moisture. In food processing facilities with frequent washdowns, higher ratings are essential. IP69K rated equipment can withstand high pressure, high temperature washdowns and harsh chemicals.

Equipment with IP69K protection keeps water and contaminants out of critical components.

This protection:

  • Improves uptime,
  • Extends equipment life, and
  • Supports contamination prevention in demanding sanitation areas.

Build a Strong Sanitation and Equipment Strategy

The strongest food safety programs combine good hygiene with the right equipment. When machinery can withstand frequent sanitation, cleaning becomes faster, safer, and more consistent.
The cost of food contamination is high. Contaminated food not only affects consumer health but also a business's brand.

Safeguard your reputation and protect your customers. Establish strong employee hygiene and sanitation procedures. Support those efforts with equipment designed to withstand demanding washdown environments. Contact the experts at LEESON Motors to find the right washdown motor for your facility.



Talk To Our Sales Team

We're here to help. Our team of experts is ready to help energy-efficiently power your business. 

 

Frequently Asked Questions About Preventing Food Contamination

What causes food contamination in processing facilities?

Bacteria, chemicals, dirty equipment, poor employee hygiene, or contaminated packaging materials can cause food contamination.

How do washdown procedures help prevent food contamination?

Washdown procedures remove bacteria, residue, and allergens from equipment surfaces. This helps maintain sanitation in food processing environments.

Why are washdown duty motors important for food safety?

Washdown duty motors can resist water and chemicals. This reduces equipment failure and contamination risks during frequent cleaning.

 

Page Updated: May 8, 2026